Other Parts Discussed in Thread: ISO5452
Hiii,
I am designing a IGBT gate driver with Texas IC ISO5500 . In my application I require higher sourcing and sinking currents, thats why i am using a external current buffer , same was attached . This circuit was
suggested in the ISO5500 datasheet, page no.34. when analyzing the buffer circuit , I am getting a voltage VEB of more than 25V across npn transitor , when below pnp transistor is in operation . But the datasheet value of VEB for the transistor is 5V only, means it will fail. Same problem for PNP transistor also , when NPN transistor is in operation. please solve my query. Let me know if anything is required.