Part Number: TUSB522P
Dear Team,
My customer used three TUSB522p on their board. We made EQ2 floating and measure the voltage, we found that the value of voltage is 0.56V only.
But the spec said that the floating voltage should be Vcc * 0.36 (typ). Vin=3.3V. Vf should be 1.188V.
And then we measured another port and get 0.54V also.
0.54V and 0.56V are lower than VIL=0.66. So our EQ2 only get 3dB, am I correct?
Thank you.
Jim