Part Number: MAX3221
Hi,
We have been using the MAX3221 device on a design for a while and have had a few occasional failures, but on a recent batch of boards the failure seem more frequent so I would like some advice to help resolve the issue.
On production test we use the RS232 port to load the firmware to a MCU via a bootloader. This is not working and it seem the MAX3221 device is not working. I have checked the V+ and V- levels and these are at 3.3V (V+) and 0.1V (V-). On a working device this is +6V (V+) and -5.5V (V-), it looks like the boost circuit is not working?
The design does use the auto shutdown feature but there is a valid signal on Rin and the Invalid output is high.
I have attached a screenshot of the schematic.
Thanks
Dave Adams