Other Parts Discussed in Thread: DS80PCI102,
Hi team,
When the DE1 and DE2 set to 0, the datasheet says the De-emphasis level is 0dB. Does it means the device doesn't apply de-emphasis to input signal?
So, if the signal with -6dB de-emphasis inputs, I can measure the output signal that is -6dB de-emphasis signal. Is that right?
The reason why I ask you is when customer uses DS80PCI102 and set DE-emphasi to 0dB, 0dB De-emphasis signal is measured on output even though input signal is applied -3.5dB De-emphasis.
Regards,
Saito