Hi There, I am designing a current loop input/output controller. I need to
add isolation to the current loop input and current loop output. I
would like to get some recommendations on the best topology for this
design as I have not designed for an industrial application before. On the input I will be using something similar to the RCV420 current
loop receiver and or building my own opamp signal processing to
interface an ADC. 1) based on this information could you recommend the
best means of isolation to the input of the processing components? On the ouput I will use some digital isolators that will run to an
ad7707 device that will drive the current loop on the output the
isolators can be powered from the AD7707 up to 5mA. 2) can you
recommend the most approprite isolation that might be used on the
output side. Attached is a basic flow diagram showing main components and isolation.