Part Number: ONET4201LD
I would like to use ONET4201LD to drive a QDFBLD-1550-5 (link) at 2 GHz. There is a couple of things I'm not sure of:
- The example schematic shows a dump resistor RD and inductor between the laser and this driver. My laser diode has already these elements in the module, so can I just connect them straight away? In other words, do these symbols in the schematic represent the built-in resistance and inductance?
- Again the example schematic shows the PD cathode and the LD anode connected together and to VCC at 3.3V. My PD seems to like 5V (still to be confirmed from them). It looks like the APC works on the current from the PD, not voltages, so could I have 5V for the PD and 3.3V for the LD?
- It surprises me that for a GHz chip there isn't even a mention for decoupling capacitors or ground planes. Of course, having them won't harm, but, does this mean they are not essential?
- Laser diodes are sensitive to voltage glitches and have the bad habit of blow up... Is there any specific requirement to supply the ONET4201LD? Will a common 3V3 linear regulator be safe enough?
- I'll probably start with a kind of custom eval board where we would like to play with things, is it safe to have multiturn potentiometers instead of resistors for setting currents? (they tend to be 'crackling' in resistance because of the wiper and contact resistance).
Regards