This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DPHY440SS: mipi signal integrity with long cable

Part Number: SN75DPHY440SS

Hi,

my customer would like to know the mipi single quality with long cable?

the current application it might need a mipi re-timer IC. But I am not familiar with this kind chipset. How and when to use this mipi re-timer IC?

Example, if the overall trace length is as the following

Option 1:  198mm in total with 2 extra connectors.

Option 2:  148mm FPC calbe without extra connectors.

or timing can’t meet? how to know if we need use this to regenerate mipi signal or not?

I have checked section 8 of datasheet, but i still not very clear if we need this kind re-timer IC.

about the data rate, please base on Data Rate (200 Mbps to 1.5 Gbps) to provide the simulation or something. we can judge this easily.

thanks.