Please note that E2E has undergone a major upgrade. Before logging in, please clear ALL your browser's cache and cookies.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD82: SN65HVD82

Part Number: SN65HVD82

Hello,

When the SN65HVD82 power up, all the input and output ports are float,  what is the Pin D  voltage value?

The input equivalent circuit is as follows, Pin D is pulled high to VCC, but the tested voltage is about 1/2 Vcc.

Best regards

Kailyn

  • Kailyn,

    You're right. If SN65HVD82 is fully powered up, D should be pulled to Vcc by internal circuitry. Can you describe the way you measure the voltage? Do you use a multimeter or scope? Where is the grounding? What's the input impedance of the equipment? Can you also check DE and REB pins?

    Regards,

    Hao

  • Hi Hao,

    Our customer used a scope and tested the value of the Pin D is about 1/2Vcc when  SN65HVD82 is fully powered up and D is float. I will confirm with the customer of the RE and DE voltage. Do you have any suggestions? 

    Best regards

    Kailyn

  • Hi Kailyn,

    The internal pull-up uses a high resistance, so the pin voltage could easily be pulled down by external leakage currents.  Do you have an estimate of the loading introduced by the measurement (e.g., multimeter input or oscilloscope probe) and anything else connected to the pin (e.g., MCU GPIO)?

    Regards,
    Max