Part Number: TCAN1044V-Q1
Hi, Is it ok to place capacitor at CANH/L line to mitigate emission? I concern if it causes violating some conformance testing.
it it is ok, what is recommended value?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1044V-Q1
Hi, Is it ok to place capacitor at CANH/L line to mitigate emission? I concern if it causes violating some conformance testing.
it it is ok, what is recommended value?
Ito-san,
Generally it is OK to place smaller capacitances on CANH/CANL to serve as RF filters. Capacitive loading does affect the timing of the CAN waveforms, though, and can introduce bit timing asymmetry (since the recessive-to-dominant transition is driven by the transceiver but the dominant-to-recessive transition is more dependent on the RC characteristics of the bus). The maximum capacitance that could be supported per node would be a function of the data rate, number of nodes, capacitive loading of wiring harnesses, and timing margin supported by the controller device. Common approaches are to use <100 pF per node to limit the impact on timing. At very high speeds like 5 Mbps it may be better to operate without additional capacitance at all.
Regarding conformance requirements - these are very varied. Many times the system-/ECU-level requirements would specify a maximum node capacitance (either single-ended or differential), though, and you should be careful not to exceed this value. Let me know if this isn't clear or if I can help provide further details.
Max