Hi team,
My customer is using TCAN1042 in 12 nodes, data rate 1M, cable line length=10m. See connection below, they have two CANs in one machine, and total 6 machines in the system. They connect two CAN They found data loss when two machine 1 and machine 6 have 120ohm terminal resistor. So they try to connect 4*120ohm resistor in the CAB bus, no data loss soon. Could you please help share me some possible root cause here? Thanks.
BR,
CL