Part Number: PCF8575
Hello,
i am using the PCF8575 in an actual pcb design. With this design i made temperature test.
For this temperature tests I used a thermocouplers directly on the case of the chip and i meassured a tmeprature of 80°C.
-> Is this temeprature ok for the chip?
I only found the ambient temperature of +85°C in the datasheet and the junction-to-ambient resistance.
But i don`t know how i canuse these definitions, because i meaussered the case temperature?
Can you help me to calculate this or can you say that the 80°C as case temperature is ok?
In an other scenario i have a temperature o 90°C on the case...is that also ok?
I hope you can help me.
Thanks and best regards
Michael