This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DPHY440SS: Compatibility with Xilinx MIPI IP

Part Number: SN65DPHY440SS


Hi,

We have designed a system that uses the SN65DPHY440SS in the same way as mentioned in sction 8.2.1 of the datasheet.  Our source of MIPI data is a Xilinx Artix 7 FPGA and the sink of the MIPI data is a Xilinx Kintex 7 FPGA.

Are there any know issues, limitations, or incompatibilities with using the standard MIPI IP provided by Xilinx?

The retimer part does not every transition into the High Speed state and remains in the Low Power state. 

We have a continuous high speed clock going to the retimer which is passing through, but no data on channels 1 or 2 is passing through.

We are satisfying the requirements for the physical interface required by the MIPI standard.

Thanks.