Other Parts Discussed in Thread: HD3SS3220, TUSB8041A, TUSB8041
Hi,
I have a Macbook Pro with 4 ports that supports all features. I fully understand that is a rather complex build, but my main problem is not that I don't have enough fully featured ports. It's rather that when you hook up SD card readers, webcams, external mouse and such, you run out of ports alltogether.
I've done an implementation of TUSB8041A with HD3SS3220 on the ports that work well at high speeds. Is there anything obvious I'm missing that prevents us from making a hub that has 1 UFP and 4 DFP - using offering Type C connectors? I understand that adding full PD to 4 ports might require a 400W power supply and that if all ports should support Alt mode, it will cost a fortune, but I'm thinking of just a hub for data.
J