This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1210: Can't interface with the 3.3V MCU ULPI interface.

Part Number: TUSB1210


Hi team

Considering the 1.8V VDDIO of TUSB1210, how could it connect to ULPI interface of 3.3V MCU such as STM32?

The competitor is USB3320, which could be interfaced with a 3.3V MCU due to the 3.6V maximum VDDIO supply of USB3320.

Do you have any advice on this opportunity?