This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP410: 480 x 272 HDMI/ DVI Transmitter

Part Number: TFP410
Other Parts Discussed in Thread: SN65LVDS311

Hello Team,

We have an application where we are driving a 480 x 272 LCD with 9MHz pixel clock from a 24 bit RGB source and want to also output the data via HDMI/DVI so that the same video stream can be viewed on an external monitor. Do we have any HDMI/DVI bridges that can be used for this application? TFP410 looked like a good candidate despite being intended for higher resolution displays, except the minimum specced input data clock is 25MHz so this will not work for this application. 

Regards,

Garret