Part Number: SN65DPHY440SS
Hello
I have a brief question about the SN65DPHY440SS, can it also be used together with an image sensor and a CPU, which each have a DPHY with the specification 1.2?
Best Regards
Kevin Keller
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65DPHY440SS
Hello
I have a brief question about the SN65DPHY440SS, can it also be used together with an image sensor and a CPU, which each have a DPHY with the specification 1.2?
Best Regards
Kevin Keller
Kevin
The DPHY440 is only DPHY1.1 compliant. The image sensor and the CPU is DPHY1.2, but should be backward compatible with DPHY1.1, and then have to run at DPHY1.1 in order to use the DPHY440.
Thanks
David