Part Number: DP83TC811R-Q1
Other Parts Discussed in Thread: DP83TC811
Hello,
we are having a strange Problem with the DP83TC811R Phy
which is connected to a lan7801. The lan7801 is connected
to a raspberrypi. We are using the Phy in Master mode.
We are facing a reconnect issue if the connected slave
is disconnected and reconnected again then the connection will
*sometimes* not be reestablished.
The strange thing is that in INT_STAT2 always "Overvoltage"
and in INT_STAT1 always "ESD Event" is set.
Also the "No Frame Detected" in INT_STAT3 is set event
there is a connection established.
Why are there NoFrame, overvoltage and ESD interrupts?
Overvoltage and ESD is almost always present.
What does overvoltage mean here? The datasheet says it's VDD. Which VDD is this?
When do you get an ESD event?
Do you think these messages are connected to not being able to sync
after the re-connect from the external interface?
I also attached our schematic.
Thanks for your help.
Best Regards,
Sven