Other Parts Discussed in Thread: MSP430F5529, , MSP430FR6989, , MSP430WARE
I'm trying to receive CAN messages using TCAN4550 and MSP430F5529. I thought the provided sample code for Code Composer Studio would be a good place to start (found here: https://www.ti.com/product/TCAN4550-Q1#design-development##software-developmentthe target to MSP430F5529 I get several "identifier is undefined" errors, preventing the code from compiling. Below are a few examples of the errors I'm getting:
"../driverlib/MSP430FR5xx_6xx/cs.c", line 115: error #20: identifier "CS_BASE" is undefined
"../driverlib/MSP430FR5xx_6xx/cs.c", line 115: error #20: identifier "OFS_CSCTL1" is undefined
"../driverlib/MSP430FR5xx_6xx/cs.c", line 115: error #20: identifier "DCORSEL" is undefined
"../driverlib/MSP430FR5xx_6xx/cs.c", line 116: error #20: identifier "DCOFSEL_7" is undefined
"../driverlib/MSP430FR5xx_6xx/cs.c", line 117: error #20: identifier "DCOFSEL_0" is undefined
"../driverlib/MSP430FR5xx_6xx/cs.c", line 120: error #20: identifier "DCOFSEL_1" is undefined
"../driverlib/MSP430FR5xx_6xx/cs.c", line 123: error #20: identifier "DCOFSEL_2" is undefined
"../driverlib/MSP430FR5xx_6xx/cs.c", line 126: error #20: identifier "DCOFSEL_3" is undefined
"../driverlib/MSP430FR5xx_6xx/cs.c", line 129: error #20: identifier "DCOFSEL_4" is undefined
"../driverlib/MSP430FR5xx_6xx/cs.c", line 132: error #20: identifier "DCOFSEL_5" is undefined
"../driverlib/MSP430FR5xx_6xx/cs.c", line 135: error #20: identifier "DCOFSEL_6" is undefined
These errors continue but with a different class name in the quotes. I would appreciate any advice on the subject. Thanks!