This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987DDK: Use as a replacement for TPS65987DDH

Part Number: TPS65987DDK

Hi,Sir

I was trying to create a board using TPS65987DDH and TUSB1046 to output TypeC_AlternateMode DP4 lanes from Displayport 1.4 input.
However, even if I look for TPS65987DDH, it is out of stock and cannot be purchased.

So I would like to do the same with TPS65987DDK instead of TPS65987DDH, is that possible?
If possible, is it possible to simply replace it? Or do you need to change the peripheral parts as well?

Best Regard

  • Hello,

    We do not recommend using the TPS65987DDK in place of the TPS65987DDH because it is for TBT applications and is different than the DDH version. I would recommend waiting for the TPS65987DDH to be back in stock and in the meantime, you can order the TPS65987EVM for testing purposes.

    Thank you,

    Hari