Part Number: DS90C189-Q1
Hi Team,
I designed a board which is included Analog Devices ADV7842, TI DS90C189. ADV7842 has 36-bit RGB outputs data but I use 24-bit RGB data output of ADV7842. 24-bit RGB data inputs DS90C189 after 3.3v to 1.8v level shifter. When I looked at DS90C189-Q1EVM, it have 50 ohm termination resistors(do not install) on RGB inputs. What is the cause of the 50 ohm resistors usage ? Should I use 50 ohm resistors on DS90C189 RGB inputs in my design ?