Part Number: TPS65994AD
Hi TI
According to datasheet, it mentions TVS is a pseudo Schottky diode but TVS utilizes the Zener diode theory to protect IC.
Why Schottky diode could be used for current surge protection?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65994AD
Hi TI
According to datasheet, it mentions TVS is a pseudo Schottky diode but TVS utilizes the Zener diode theory to protect IC.
Why Schottky diode could be used for current surge protection?

Hi Eddie
Schottky diodes are used on VBUS to help absorb large GND currents when a Type-C cable is removed while drawing high current. The inductance in the cable will continue to draw current on VBUS until the energy stored is dissipated. Higher currents could cause the body diodes on IC devices connected to VBUS to conduct. When the current is high enough it could damage the body diodes of IC devices. Ideally, a VBUS Schottky diode should have a lower forward voltage so it can turn on before any other body diodes on other IC devices. VBUS could ring below GND which could damage devices hanging off of VBUS. The Schottky diode will start to conduct once VBUS goes below the forward voltage. A TVS diode can also act as a “pseudo schottky diode” as they will also start to conduct when VBUS goes below GND.
The main purpose of the TVS Diodes is to help suppress and clamp transient voltages. Most TVS diodes can fully clamp around 10 ns and can keep the VBUS at their clamping voltage for a period of time. Looking at the clamping voltage of TVS diodes after they settle during a transient will help decide which TVS diode to use. The peak power rating of a TVS diode must be able to handle the worst case conditions in the system.