This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDMI to LVDS converter

Hi, I'm looking for a device which can take HDMI ( HDMI 1.4) input and provide LVDS output for driving a LCD panel.

The LCD specifications are

1. Interface : LVDS ( 1 Port)

2. Pixel - H: 1280 x 3 ( R G B) ; V : 768

3. Clk Frequency : 68.3 MHz

Please suggest the suitable device. Thanks