I want to use the TLK2711-SP in single operation. In orther words, one TLK2711-SP only transmit the serial data, and another TLK2711-SP only receive the serial data. In this case, how should I deal with the unused pins? Especially with the RXD, RXCLK, RXN, RXP, TXD, TXN, TXP, would it be better if I pull up or pull down these unused pins?
And, by the way, some engineers told me that the PLL in the TLK2711 is sensitive to jitter in the range of 300KH to 3MHz. Does it means the GTX_CLK's is acceptable if its jitter is slower than 40ps in the range of 300KHz to 3MHz?
Thanks for your help.
Liang Li