Hello,
I need to double-check compatibility of the DS90UB913 with the OV10635 Megapixel camera. Below is a link to the spec sheet:
http://www.ovt.com/download_document.php?type=sensor&sensorid=115
The output interfaces from the camera are 10-bit DVP, which appears to be supported after looking through the DS90UB913 datasheet. It also lists output formats of up to 18-bit combined RAW, or separated 10-bit RAW and 8/10-bit YUV422. Can the DS90UB913 still support this output format? My guess is that it does.
Thanks,
Luis Cordova