Other Parts Discussed in Thread: SN65MLVD082, SN65MLVD204B, SN65MLVD206B, SN65MLVD206, SN65MLVD200
art Number: SN65MLVD082
Dear Technical Support Team,
SN65MLVD082 datasheet shows it is possible to implement 32 nodes(max) with multipoint topology.
Could you share TI's result and topology of IBIS simulation for 32 nodes?
If you have the result of other device like SN65MLVD204B and SN65MLVD206B, could you share them?
I'd like to know which do you simulate type1 or type2.
Our customer has been trying IBIS simulation with 19 nodes, however their result is not good.
So they'd like to refer TI's topology which is satisfied with 32 nodes.
■Condition of simulation
Node: 19 node
Termination register: 100Ω for the both ends
Line length : Approximately 420mm
Driver: Implement center of topology
Target IBIS model: SN65MLVD082
Simulation tool: signoise (Cadence)
Best Regards,
ttd