[ DS90UB964-Q1 ] MODE pin and IDx pin
Hi,
Can you please elaborate how MODE and IDx pin define the mode upon power-up?
As my understanding, these pins (MODE and IDx) have ADC internally. Once device is powered-up (i.e, supply voltage goes into the valid range),
these adc start to read and conver the voltage, applied to each pin to digital word, then device change the mode based on that digital read out.
Or it's really appreciated if you can share the internal equivalent circuit drawing.
Also, the circuit schematics of EVM suggests to put 0.1uF cap for these pins.
Are these for having more robustness to interference?
What we shuld not do here is to haveing too large cap, because time constant getting larger and takes longer time to stable the voltage.
Thanks,
Ken
Similar Post, posted almost same time.
DS90UB921-Q1: IDX, MODE pin 0.1uf capacitor
http://e2e.ti.com/support/interface/high_speed_interface/f/138/t/649083