This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: How to output a 1280x720@30fps color bar base on csi0 4 lane 10/12 bit RAW

Part Number: DS90UB953-Q1


how can i output  yuv422 1280x960@30fps color bar?

  • Hi,
    please refer to d/s page27, you should configure some key parameters as below. for your YUV422_8_8 case, the block size can be set as 2.
    PGEN_ACT_LPF – Number of active lines per frame
    • PGEN_TOT_LPF – Number of total lines per frame
    • PGEN_LSIZE – Video line length size in bytes. Compute based on pixels per line multiplied by pixel size in
    bytes
    • CSI-2 DataType field and VC-ID.
    • Optional: PGEN_VBP – Vertical back porch. This is the number of lines of vertical blanking following Frame
    Valid.
    • Optional: PGEN_VFP – Vertical front porch. This is the number of lines of vertical blanking preceding Frame
    Valid.
    • PGEN_LINE_PD – Line period in 10-ns units. Compute based on Frame Rate and total lines per frame.
    • PGEN_BAR_SIZE – Color bar size in bytes. Compute based on datatype and line length in bytes (see details
    below).

    example as below:
    example1 (shown in d/s):
    #Patgen RGB888 1920x1080p30 Fixed 8 Colorbar
    WriteI2C(0xB0,0x00) # Indirect Pattern Gen Registers
    WriteI2C(0xB1,0x01) # PGEN_CTL
    WriteI2C(0xB2,0x01)
    WriteI2C(0xB1,0x02) # PGEN_CFG
    WriteI2C(0xB2,0x33)
    WriteI2C(0xB1,0x03) # PGEN_CSI_DI
    WriteI2C(0xB2,0x24) # RGB888
    WriteI2C(0xB1,0x04) # PGEN_LINE_SIZE1
    WriteI2C(0xB2,0x16)
    WriteI2C(0xB1,0x05) # PGEN_LINE_SIZE0
    WriteI2C(0xB2,0x80)
    WriteI2C(0xB1,0x06) # PGEN_BAR_SIZE1
    WriteI2C(0xB2,0x02)
    WriteI2C(0xB1,0x07) # PGEN_BAR_SIZE0
    WriteI2C(0xB2,0xD0)
    WriteI2C(0xB1,0x08) # PGEN_ACT_LPF1
    WriteI2C(0xB2,0x04)
    WriteI2C(0xB1,0x09) # PGEN_ACT_LPF0
    WriteI2C(0xB2,0x38)
    WriteI2C(0xB1,0x0A) # PGEN_TOT_LPF1
    WriteI2C(0xB2,0x04)
    WriteI2C(0xB1,0x0B) # PGEN_TOT_LPF0
    WriteI2C(0xB2,0x65)
    WriteI2C(0xB1,0x0C) # PGEN_LINE_PD1
    WriteI2C(0xB2,0x0B)
    WriteI2C(0xB1,0x0D) # PGEN_LINE_PD0
    WriteI2C(0xB2,0x93)
    WriteI2C(0xB1,0x0E) # PGEN_VBP
    WriteI2C(0xB2,0x21)
    WriteI2C(0xB1,0x0F) # PGEN_VFP
    WriteI2C(0xB2,0x0A)

    #Patgen YUV422 1280x960p30 Fixed 8 Colorbar
    WriteI2C(0x33,0x03)
    WriteI2C(0xB0,0x00) # Indirect Pattern Gen Registers
    WriteI2C(0xB1,0x01) # PGEN_CTL
    WriteI2C(0xB2,0x01)
    WriteI2C(0xB1,0x02) # PGEN_CFG
    WriteI2C(0xB2,0x32)
    WriteI2C(0xB1,0x03) # PGEN_CSI_DI
    WriteI2C(0xB2,0x1E) # YUV422_8_8
    WriteI2C(0xB1,0x04) # PGEN_LINE_SIZE1
    WriteI2C(0xB2,0x0A)
    WriteI2C(0xB1,0x05) # PGEN_LINE_SIZE0
    WriteI2C(0xB2,0x00)
    WriteI2C(0xB1,0x06) # PGEN_BAR_SIZE1
    WriteI2C(0xB2,0x01)
    WriteI2C(0xB1,0x07) # PGEN_BAR_SIZE0
    WriteI2C(0xB2,0x40)
    WriteI2C(0xB1,0x08) # PGEN_ACT_LPF1
    WriteI2C(0xB2,0x03)
    WriteI2C(0xB1,0x09) # PGEN_ACT_LPF0
    WriteI2C(0xB2,0xC0)
    WriteI2C(0xB1,0x0A) # PGEN_TOT_LPF1
    WriteI2C(0xB2,0x04)
    WriteI2C(0xB1,0x0B) # PGEN_TOT_LPF0
    WriteI2C(0xB2,0x65)
    WriteI2C(0xB1,0x0C) # PGEN_LINE_PD1
    WriteI2C(0xB2,0x0B)
    WriteI2C(0xB1,0x0D) # PGEN_LINE_PD0
    WriteI2C(0xB2,0x93)
    WriteI2C(0xB1,0x0E) # PGEN_VBP
    WriteI2C(0xB2,0x21)
    WriteI2C(0xB1,0x0F) # PGEN_VFP
    WriteI2C(0xB2,0x0A)


    best regards,
    Steven
  • thanks for your quick reply ,i have a try !!!