This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD09: RS422 side_B, & TTL@3.3level IO side_A

Part Number: SN65HVD09


Multiple RS422 signals are to be terminated in FPGA.

Using the SN65HVD09 transceiver, Side A gives the TTL output which are to be terminated on FPGA IO pins & this is a 5V part.

The Question is whether we need to use a level shifter on side A for all TTL out??? to connect to FPGAs? .

FPGA  IOs are at 3.3 max

-Sathiyanathan