Other Parts Discussed in Thread: TUSB211, USB-REDRIVER-EVM
Hi,
I developped a small board which interface a TUSB211, two USB connectors and a voltage regulator to convert one side's VBUS to the TUSB211 necessary 3V3 power supply (see attached schematic).
I'm doing some eye diagrams with an appropriate Agilent scope and a host generating test packets.
The TUSB211 has no effect; I compared with a board without the TUSB211 and it does not change a thing.
I also tried with various value of EQ resistor, still no effect.
ENA_HS and CD are always at 0V, so is VREG.
Toggling the RST pin also has no effect.
Any help would me very appreciated.