Part Number: TUSB8041
I am trying to calculate the require power for this 12 port hub. In the TUSB8041 data sheet section 7.7 there is some parameter so with that information I am trying to estimate base on my configuration and connected devices.
All my connected devices will be USB2.0 and according to the datasheet if my host is USB2.0 and my connected devices are USB2.0 the current drawn from the TUSB8041 is 3.3V @ 76mA and 1.1V @ 86mA. What I don't know (not on the data sheet) is what happens when you cascade the TUSB8041.
For example, if my host supports USB3.0 and USB2.0 and I have two TUSB8041 cascaded and all my connected devices are USB2.0, is it true that the two TUSB8041 will be working in "USB2.0 mode"? If true, is the current drawn for each TUSB8041 will be 3.3V @ 76mA and 1.1V @ 86mA plus the current drawn by the connected devices?
Thank you,
Jeremy