Part Number: ISO7041
Other Parts Discussed in Thread: SN6501, SN6505B, ISOW7741
Hello
I need your help
I have conneted a ISO7041 to my board
I have one Power supply connected to the VCC1 ( Pin number 1) I have connected all other GND as well as the EN to the GND ( I use the ISO7041 F type)...
But from some reason I dont get any power on th eVCC2 ( Pin number 16 ) which is the Isolated
As far as i know , I need to connect a 3.3V on the Non Isolated pin and the ISO7041 should make a 3.3_ISO
Please advise