Part Number: ISO6741
Other Parts Discussed in Thread: ISO7841, ISO7741
Similar question for the ISO6741. Can you please let me know if the carrier frequency is the same for ISO6741 (450MHz).
Thank you,
Oliver
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Oliver,
Thank you for posting to E2E! ISO6741, along with ISO7741 and ISO7841, employs OOK architecture where a carrier frequency of ~450MHz is used to modulate input signals and transmit them across the isolation barrier.
Please let us know if you have additional questions.
Respectfully,
Manuel Chavez