Part Number: ISO7741DBQEVM
Other Parts Discussed in Thread: ISO7741, PSPICE-FOR-TI
Hello,
The following questions are:-
1. I want to calculate signal transfer bandwidth for the Digital isolator- ISO7741 but the parameters are missing from the datasheet.
2. The PSPICE simulation model available for ISO7741 is not working. It is giving as : Can't find the definition of model "DBREAK".
Simulation software: LT-SPICE.
Thanks and Regards
Ashish Nawani