This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7021: Can the ISO7021 perform logic translation between a 1.8V supply and a 3.3V or 5V supply?

Part Number: ISO7021


The datasheet recommend operating conditions suggest that if one side is at 1.8V supply, then the other side can only be between 1.71 -> 1.89V. 

Does this mean that it will not work with a 1.8V supply and a 3.3V supply, or am I misunderstanding this table?