This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7720-Q1: prime side lose power and secondary side output

Part Number: ISO7720-Q1


In the datasheet desicribe‘In the event of input power or signal loss, the default output is high for devices without suffix F and low for devices with suffix F." my question as follows:

1. use ISO7720-Q1 design, without suffix F, if the prime side of the chip  lose power(eg:5V), are the secondary side of pin 6 and pin 7 still outputs high level either on or off?