Part Number: ISO7420FE
Other Parts Discussed in Thread: ISO7420
The datasheet for the ISO7420FE specifies operation of both the input and output down to 3V. Assuming the input side is powered to 5V with a logic low on the input. Is it possible that the output could glitch high during power down of the output VCC2? If so, at what level of VCC2 could a glitch occur. If glitches can occur, are there any recommendations to mitigate this such as a pull down resistor on the output.
Stated differently, is there any POR type function on VCC2 such that the outputs of the ISO7420FE will be guaranteed to be in a logic low state during VCC2 power down with VCC1 powered. I am looking for additional insight into what is noted in Table 2 of section 8.4 of the device datasheet.