Other Parts Discussed in Thread: SN6505A,
Hello:
It would appear that the operation of SN6505A up to 6.5 V would be very beneficial.
Its max is 7V
So could this be used safely up to 6.5v max...in reality, seems most will have 6.25v to convert to some isolated lower floating voltages.
If this cannot be specified, is there a similar SOT23-5 pin device that can?
r