Other Parts Discussed in Thread: ISO1640
We are looking to replace the SI8600, we have used the SI8600AC-B-ISR.
We need,
Minimum Isolation Voltage: 1500Vrms
Minimum Creepage: 2.9mm
Minimum Clearance: 2.3mm
Must have a UL certification
This Ti part looks like a good fit, however,
It is somewhat different in-terms of the logic levels values that determine whether a signal is low or high.
Is this the best part for the application, or are there others more suited.
thanks,