This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7760: The ISO7760DBQR Out of stock, is there any alternative parts?

Part Number: ISO7760


Hi TI team.

The ISO7760DBQR has been out of stock for a long time in market, is there any pin to pin part can replace it?

Thanks.

  • Hi Tsai,

    Thanks for reaching out.

    Currently, ISO7760DBQR is the only 6-channel device with 6/0 channel configuration available in DBQ package. We do not have any other device to offer as a pin-compatible alternative.
    If a redesign is possible, then the closest alternatives would be ISO7760DWR or ISO6760DWR which are available in larger DW package. Thanks.


    Regards,
    Koteshwar Rao