Other Parts Discussed in Thread: ISO3080, , ISO1452, ISO1412, ISO1432
Good morning,
we usually mount on our products as RS485 transceiver the ISO3080DWR.
Following the schematic
The ISO3080DWR is a full duplex tranceiver, but we are using it in HALF DUPLEX MODE.
Now, for availability reasons, I'm evaluating the ISO3082DWR (which is an half duplex).
Following the pinout difference:
What does the datasheet mean for pin 11 and pin 14?
Are not internally connected and so I can use my PCB (without modifications on the external connections)?
Or connecting pin11 with pin 14 and pin 12 with pin 13 the ISO3082DWR doesn't work correcty or it is possible to damage it?
Please let me know as soon as possible.
Best regards.
Diego Bolzoni