Part Number: ISOUSB211
Hi,
I am evaluating ISOUSB211DPEVM for USB Audio use where the ISOUSB211DPEVM is inserted in between the path of music streamer USB output (type A) and USB DAC input (type B). Another competing product is ADUM4166. Subjective comparison was made against FCPGA-based Intona 7055-C USB Isolator.
Why is the default PCB configuration not to use the external 3.3V linear voltage regulator but instead use internal LDO to generate 3.3V from VBUS? Is this the more optimal configuration? Why waste the external voltage regulator? And the need to desolder / add connections to change its configuration. Using jumpers should be better. Having terminal blocks for connecting external DC power to the PCB makes more sense.
The competing product ADUM4166 uses external 24MHz crystal/clock for retiming. What is the clock source for ISOUSB211?
Thanks,
Anwar