Part Number: ISO1432
Dear Team ,
Please find our Block diagram of our system. We facing issue when multiple slave of ISO1432 in half duplex...

In our system when HMI send request to two salves, only one slave able send and receive information to master (HMI). another slave able to receive request from master (HMI) but not transmit correct data..
we able to receive request in both slave but out of 2 anyone of slave is able transmit data .. the other one when we debug all data are correct placed in buffer , but while transmit when we see in serial analyzer its show,, data always zero..
for example 16 array..
working slave..
001 002 015 010 020 100 060 000 000 000 000 000 000 000 000 000 018
Problematic slave
000 000 000 000 000 000 000 000 000 000 000 000 000 000 000 000 000
Please note that while transmitting frame size matching in both slave.. but problematic slave data is zero zero..
we cant judge the slave which one working... suppose slave1 power on and slave two power on after sometime slave 1 working...
suppose slave2 power On frist and slave 1 power after sometime slave 2 working... Please find circuit below.
Thanks in advance fot your support and guidance
Rgds
Ajay S