Other Parts Discussed in Thread: ISO1212, ISO1211
Hi All,
currently we are using optocoupler HCPL-063L to isolate our digital inputs.
And our input signals are 24V.
Do you have a solution with digital isolator that can support 24V input and 3.3V output ?
From the input side we only have 24V signal and GND and no power.
If you don't have digital isolator that can direct support 24V , maybe a combination of level translator from 24V to 3.3V and then digital isolator with integrated power?
Best Regards,
David.