Part Number: ISO7821
Other Parts Discussed in Thread: ISO721
Dear Technical Support Team,
<Question 1>
Malfunction (reversal of output logic) assuming that there is no abnormality in the input signal or power supply voltage
Please let me know if there are any factors that may cause it.
We understand the risk of malfunction at CMTI> 150kV / us.
For example:
strong electric field over xxx kV/m
strong magnetic field on xxx μT
under xxx input signal dv / dt
I find following documentation about old digital isolator . Is it useful for ISO7821?
Digital Isolator E-Field Sensitivity
ISO72x Digital Isolator Magnetic-Field Immunity
https://www.ti.com/lit/an/slla181b/slla181b.pdf?ts=1649900867212
<Question 2>
I would like to know in detail the signal transmission method and principle to the extent that it can be disclosed.
(How to maintain the output H when the input signal is H, etc.)
From this content, it is best to say that the malfunction factor is limited to the unrealistic mode if CMTI is satisfied.
I see this documentation and this is useful for understanding signal transmission method
1.2 On-Off Keying (OOK) Based Communication
www.ti.com/.../slla284d.pdf
<Question 3>
If there is a document that compares the malfunction tolerance with a magnetically coupled isolator or a signal transmission method using pulse transformer.
Would you please provide it? In particular, it is desirable to have comparative materials with the pulse transformer method.
Best Regards,
ttd