Part Number: ISO3088
Other Parts Discussed in Thread: ISO1430, ISO1450
Dear all,
We have used the ISO3088 in previous designs with both Vcc1 and Vcc2 supplied by 5 V.
However, in our current design we are suppliyng Vcc1 with 3.3 V, and we noticed that the communication stops after some time.
We probed the receiver output (R) signal and we noticed a level shift when the problem happens.
In the images attached you can see that initially we have a signal with 3.3V, peak to peak, and then suddenly it halves.
Could you give us an insight of what may cause this behaviour. The ISO3088 is connected directly to the UART of the microcontroller
Thank you in advance.