Part Number: ISO1430
Other Parts Discussed in Thread: ISO1450,
Hello,
I am selecting a isolated half-duplex rs485 transceiver with our requirement specified 1 Mbps Data rate needed.
I see ISO14xx series fits our application. What I see from TI website and some other distributor that the ISO1430 and ISO1450 have the same price even though ISO1450 can support higher data rate than ISO1430. So in our case which only 1 Mbps is required, which one shall I choose between ISO1430 or ISO1450, considering that they have the same price.
Thanks