Other Parts Discussed in Thread: SN6507
Hi Team,
Could you help our customer's concern. I have posted their inquiry below.
I have a device that outputs 3~4.2VDC. Can I use the following topology to get around 30~42VDC
the vin is 3VDC to 4.2VDC not 12VDC. i HAVE TWO QUESTIONS BACK TO BACK i WANT TO ASK YOU
Output is 200mA
ratio of transformer is 1:10
Name of transformer: 750032051 link: https://www.we-online.com/catalog/datasheet/750032051.pdf
I have a second question
using the same topology, I have a device that outputs 12VDC @ 1A. I would like to isolate the 12VDC to output dual 5VDC
The first one. Input 3~4.2VDC @ 200mA Expected output 30~42VDC
The second one. Input 12VDC @ 1A Expected output dual outputs of 5VDC
Please see attached file:
Best regards,
Jonathan