Part Number: ISO6742
Hi,
has the ISO6742 any requirement at its iputs regarding the maximum risetime?
or has he schmitt trigger inputs?
thanks
chris
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO6742
Hi,
has the ISO6742 any requirement at its iputs regarding the maximum risetime?
or has he schmitt trigger inputs?
thanks
chris
Hi Chris,
Thanks for reaching out.
Yes, the input of most of our digital isolators are Schmitt trigger inputs including the ISO6742. One way to identify if the inputs are Schmitt trigger inputs is by looking to see if the input thresholds have a hysteresis. I am copying below a screenshot of datasheet showing input thresholds along with hysteresis.

There is no restriction on the input signal rise time to ISO6742 inputs. The signal rise time can be as fast or slow as it can be, there is no upper or lower limit. Thanks.
Regards,
Koteshwar Rao