This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO224BDWVR

Other Parts Discussed in Thread: ISO224

Hi All,

I am planning to use ISO224BDWVR for sensing AC voltage of peak magnitude 650 V. But I see from the data sheet that it only has provision for positive supply from 5 V to 12 V. However, the analog input supply voltage range is from -15 V to 15 V. Please suggest whether I can sense AC voltage using ISO224BDWVR. If yes, please share some simulation waveforms mentioning the supply voltage and the input analog voltage.