Part Number: ISO1540
Other Parts Discussed in Thread: ISO1640
Hi expert,
Customer used ISO1540 for i2c and in order to verify the part can support bi-direction, they did two tests;
case1: side1 connects to PSE_I2C, side2 connects to MCU_I2C

case2: side1 connects to MCU_I2C, side2 connects to PSE_I2C

To be clear, there is no communication issue.

Could you please explain why the low level are different and the time period of low level are different as well?
Regards,
Allan